AnsweredAssumed Answered

Calibration using port extension

Question asked by zubairrafiq on Mar 13, 2010
Latest reply on Mar 13, 2010 by Dr_joel
I want to incorporate two cables in calibration  as shown in fig 1 .
First of all I connection each cable to each PNA cable as shown in fig 1
Image
After setting all channel parameters I used calibration 2port & then unknown through.
Then I simply remove calkit as shown in fig  and use unknown through as shown in fig 2
Image
Please tell me weather  I m doing right or wrong.
if Not what could be other possible way.

Hardware = PNA 8363B
Operating Frequency 1.5G 1.6G

Regards
Muhammad Zubair Rafiq  

Attachments

Outcomes