AnsweredAssumed Answered

What is the mathematical form of dynamic accuracy curves?

Question asked by b.d.hall on May 19, 2011
Latest reply on May 20, 2011 by b.d.hall
There are curves for dynamic accuracy in the The Technical Specifications for the E836xB NAs, among other things. These curves can also be calculated using Agilent's na_calculator.

The Technical Specifications contains a link to a description of equations used to generate the uncertainty curves in the specs., however, there are no equations there for dynamic accuracy.

My question is this: can the mathematical form of the DA curve be described in terms of instrument specs., or parameters?  

Outcomes