AnsweredAssumed Answered

Re-draw function

Question asked by MIKAELGARCIA on Sep 23, 2004
Latest reply on Sep 24, 2004 by MIKAELGARCIA
I noticed that when I change the dimension of an object in Momentum, the location of my reference offsets do not get updated. However, if I go in to the Port Editor and just hit OK they are re-drawn in the correct locations. Do I have to manually update the offsets like this or can I just ignore the location shown in the display? The reason I am asking is that it is time consuming to do this on all ports as soon as I make a change. My offsets stay the same all the time so I am guessing this is just an issue with the re-draw function. Insight into this would be welcome. (ADS 2003C).  

Outcomes