AnsweredAssumed Answered

Question on EVMWithRef component

Question asked by COMMIT on Sep 9, 2003
Latest reply on Jan 13, 2005 by WSTR
I am using EVMWithRef model for EVM measurement, but can not understand the setting and effect of the parameters:
1. SamplePerSym is needed?
2. Can EVMWithRef do synchronize between Ref and test signal? Can it adjust the delay between the two signal even though the delay difference is less than one sample?
3. If SampPerSym is not zero (for example=4), how does EVMWithRef know which sample is the actual sampling point, for the EVM should only be measured at the sample point?  

Outcomes