AnsweredAssumed Answered

Import Loadpull Data using Loadpull Design Guide

Question asked by efranzwa on Aug 23, 2004
Latest reply on Mar 1, 2006 by nickmmw
Need help importing Focus load pull data into ADS 2003A.  When I import a .LPD file using the Design Guide, the plotted impedances are too high.  My loadpull data file is in the un-normalized real/imaginary format.  For example, in my file, the point R + jX = 4 + j0 is being plotted at approximately 55 + j0.  I have tried changing the normalization impedance up and down by factors of ten, but can not get impedance to plot correctly.  I can email my file if someone can help.  

Outcomes