AnsweredAssumed Answered

I'm missing something?

Question asked by dbengtson on Mar 6, 2006
Latest reply on Mar 14, 2006 by dbengtson
Hi:

I'm running a simple Ptolemy simulation. I'm running the FM timed signal source into a timed sink. I'm using the default parameters for the FM source. When I  run the simulation, and plot the frequency spectrum of the output, I get an appropriate FM modulated signal, but it's centered at 0Hz, instead of 1 MHz. I'm doing something incorrect, but I'm not quite sure.

Thanks
Dave  

Outcomes