I am working with ADS 2004A and run into what I perceive as an issue:
When selecting Positive and Negative noise nodes, it is impossible (I think) to get rid of the negative noise node and leave only the positive. In other words, if I accidentally click on a negative noise node, I can't get rid of it short of selecting everything else in the design other than NoiseCons and putting them into the new schematic window and then retyping all the NoiseCon info. Not too cool if you have 50 NoiseCons in the circuit. Help.
When selecting Positive and Negative noise nodes, it is impossible (I think) to get rid of the negative noise node and leave only the positive. In other words, if I accidentally click on a negative noise node, I can't get rid of it short of selecting everything else in the design other than NoiseCons and putting them into the new schematic window and then retyping all the NoiseCon info. Not too cool if you have 50 NoiseCons in the circuit. Help.
In the meantime the workaround would be to delete the NoiseCon that you have accidentally added a negative node to and reinstantiate a new NoiseCon in it's place. Â :-/