Hello,
I´ve got a problem which is driving me mad right now. I got some coupled lines and want to build up a filter. If all is in a straight line there`s no problem. Now I wanted to build a waveguide in Momentum and tried to rotate the layout components by 15 degrees. Since then there are gaps everywhere and my filter doesn´t work anymore. So I tried to reduce the resolution so that the mesh won´t regognize the gapa and sometimes it works.
But my most urgent problem is if I want to build the filter on a substrate I need an GDSII-File. And there the gaps keep appearing, no matter what resolution I use.
Can someone please help me???!!
Many Thanks!!!
I´ve got a problem which is driving me mad right now. I got some coupled lines and want to build up a filter. If all is in a straight line there`s no problem. Now I wanted to build a waveguide in Momentum and tried to rotate the layout components by 15 degrees. Since then there are gaps everywhere and my filter doesn´t work anymore. So I tried to reduce the resolution so that the mesh won´t regognize the gapa and sometimes it works.
But my most urgent problem is if I want to build the filter on a substrate I need an GDSII-File. And there the gaps keep appearing, no matter what resolution I use.
Can someone please help me???!!
Many Thanks!!!
flattening merging and then rotating the structure didn´t work, because there are problems with the grid snap if I want to rotate the whole structure. But flatting the already rotated single coupled lines and then moving them just a little bit and then merging did work.
Thank you for your christmas present answer.
Robert