I'm trying to retrieve data off of the E4440A as fast as I can. I configure the analyzer and the sweep time is about 2.6 seconds. When I read back the data it takes about 5.5 to 6 seconds to take a sweep and plot the data. It shouldn't be taking that long should it?
Span 10 MHz
Points 101
Atten 0 dB
VBW 200 Hz
RBW 300 Hz
Manual FFT ON
FFT/Span 11 points
I use the following SCPI commands to read back the data.
:INIT:CONT OFF
:INIT IMM;*WAI
:TRAC:DATA? TRACE1
Thanks!
Span 10 MHz
Points 101
Atten 0 dB
VBW 200 Hz
RBW 300 Hz
Manual FFT ON
FFT/Span 11 points
I use the following SCPI commands to read back the data.
:INIT:CONT OFF
:INIT IMM;*WAI
:TRAC:DATA? TRACE1
Thanks!