AnsweredAssumed Answered

How to have N9320B default to LAN I/O on power up

Question asked by swanston on Dec 9, 2010
Latest reply on Dec 14, 2010 by demry
Is it possible to configure a N9320B Spectrum Analyzer to default into LAN I/O mode on power up rather than USB mode?  

We use this unit remotely where it is installed at a mostly unmanned site.  Should the unit ever power cycle, it requires a human to press some buttons on the front panel to put it back into remote LAN control mode.  This isn't ideal.

Apologies if I've overlooked anything in the manual but I couldn't find any reference to setting the default I/O mode following a power cycle.

Thanks.  

Outcomes