AnsweredAssumed Answered

Carrier to Noise measurement and data logging

Question asked by thomas78 on Aug 17, 2010
Hi,

I need to do CNR, carrier to noise measurement from a remoted site, and also data logging over days.

Can fieldfox do the job? i need to do rainfall analysis between 2 satelite link.

Application is simple, i just marker the peak of the waveform when no rain, then to measure and log any drop in ampitude level during raining period.

I saw from some post that there is a data link software which i can link my PC to fieldfox for data transfer.

How big is the memory capacity of fieldfox? i may need more than 1 week of data each time during deployment.

My frequency of interest is between 950 MHz to 2150 MHz which is being down convert from satelite frequency.

Analysis bandwidth is 4 MHz.

Can anyone help? Thanks.  

Outcomes