AnsweredAssumed Answered

Can I use Agilent E6474A?

Question asked by michaell on Jul 14, 2009
Latest reply on Jul 21, 2009 by sberrey
Hi,
I have device that is connected to M2M GPRS modem and this GPRS modem transmits the information to the cellular base station. I want to monitor and obtain the information such as signal quality and signal strength of the received base station; cellular ID that the GPRS modem is current connecting to; and numbers of packet being received / dropped.
Can I use Agilent E6474A and if this is an appropriate tool to be used for this testing? Otherwise, please advise which T&M tool that I need to use.
Thanks.  

Outcomes