AnsweredAssumed Answered

Can N9340B be controlled with a handheld PDA?

Question asked by irad002 on Jun 19, 2009
Latest reply on Jul 21, 2009 by JianKang
Hi,

I want to connect N9340B to a handheld PDA (probably Trimble Recon) running Windows Mobile.
The connection will probabaly be established through USB.

I intend to run a Labview application on the PDA that sends SCPI commands to N9340B through NI VISA.
I am sure that Windows Mobile can host a Labview application. However, I am not sure that Agilent IO drivers will
run on Windows Mobile. I've read the datasheet for the Agilent IO library. It says that Agilent IO connects well
with NI VISA, but the only platform that is mentioned is a PC running Windows XP, Windows 2000 etc.

Can a PDA with Windows Mobile run Agilent IO? Any other problems I am likely to encounter in this setup?

Thank you

Ivan  

Outcomes