AnsweredAssumed Answered

2.92mm vs 3.5mm calkit

Question asked by bar28 on May 14, 2009
Latest reply on May 28, 2009 by bar28
I have Agilent 8722ES (50MHz-40GHz) analyzer with 3,5mm teport cables and i would like to make measurement calibration up to 26.5GHz. I know that ideal configuration is to use 3.5mm calkit, but i have also precision 2.92mm (K) calkit which is  mechanicaly compatible with 3.5mm. What possible errors or uncertainties 2.92mm calkit would cause comparing 3.5mm calkit if i want make full two port or one port measurement calibration end of 3,5mm testportcable(s)?  

Outcomes