AnsweredAssumed Answered

Newbie...Calilbration on use of averaging

Question asked by JPA on May 8, 2009
Latest reply on May 8, 2009 by Dr_joel
euipement 8722es

I did a response cal with WR42 waveguides at 24GHz to 34GHz back to back...S21 scale/dIV at .1, @401 pts, average off and I"m getting a ripple reading of about .2, on or off with averaging, but when i cal with averaging on, I get less than .1


What is the correct way of calibrating using averaging? on or off?  

Outcomes