AnsweredAssumed Answered

VSWR at K-connector/SMA Reference Plane

Question asked by marco_toulouse on Apr 9, 2009
Latest reply on Apr 12, 2009 by odanzy
Hello,
In space applications above 20GHz, the 2.92mm connector is widely used because it is said to be compatible with the SMA, what the 2.4mm is not.

I know that the VSWR at 3.5mm/SMA is above 1.15 above 20GHz, and even 1.2 for SMA to SMA connections.

What about K-connector/SMA?
Has anybody got a chance to measure it before?

Thanks  

Outcomes