AnsweredAssumed Answered

HP 8510C cable stability

Question asked by bar28 on Apr 29, 2010
Can someone explain me, how can i measure and define in practicaly HP 8510C's cable stability parameters Cable Refl Mag Stab Port1 (Crm1) and Cable Trans Mag Stab Port1 (Ctm1)? I assume, that Ctm1 parameter i can check using testport cable which i have ended for short (i can bend the cable for example 10 different positions and after that calculate standard deviation from S11 Mag(lin) values). Of course i have made firstly one port calibration direct into test set testport 1.
More advices needed for Crm1 measurements and how to do it?  

Outcomes