AnsweredAssumed Answered

TRL calibration for x-band waveguide

Question asked by NCCU1990 on Oct 3, 2008
Latest reply on Oct 4, 2008 by Dr_joel
I want to do some measurements using x-band waveguides but I'm a bit confused about how to realize a TRL calibration.
In particular:
- Trough: can I just connect directly the flanges of the two assemblies where I want to define my reference planes?
- Reflect: can I use a shorting plate on the above mentioned flanges?
- Line: what should I use for the line (band of interest is 8.4GHz - 12.4GHz)?
- Line-2: instead of a line can I use a termination as the Flann 16100?
Thanks a lot,
regards  

Attachments

Outcomes