AnsweredAssumed Answered

GPIB controlled calibration with 85032B

Question asked by PsychoDave on Mar 4, 2008
Latest reply on Mar 5, 2008 by PsychoDave
Hello.

I am programming with VBA in Excel to control E5071C via GPIB for an automatic measurement. This starts up with a 2-port calibration of E5071C, for this I use 85032B. When I select 85032B/E as cal kit on E5071C there are two options for open/short reflection, male or female.

For controlling this on GPIB I use the following command when I would like to test open on port 1.
:SENS1:CORR:COLL:OPEN 1
This selects the first option which is male and I would like to use female since this is what I use. Are there any commands I can use to select female instead of male?

BR, David  

Outcomes