AnsweredAssumed Answered

Chnging the calibration settings

Question asked by kalai on Feb 24, 2008
Sir,
I did a full two port calibration with the following settings on the network analyzer(8753ES)
Frequency range-  0.5MHz-6GHz
Power-  -10dBm
Number of points-1601
If Band width-3.6kHz
But I wanted to change the settings after calibration.Is it advisable to change the cal settings?.What would be the measurement accuracy throughout the calibration range after changing any of these settings?
Or is it allowable to change only some of these settings without much compromise on the measurement accuracy?.
Does the change of settings is very sensitive to measuring particular kind of devices.For example,Amplifiers,Filters.
Thanks,
Kalai  

Outcomes