AnsweredAssumed Answered

In-Fixture TRL Calibration

Question asked by sri_hsr on May 7, 2008
Latest reply on May 14, 2008 by dgun
Hi All,

I want to measure Inductance and capacitance of the SMD components. I am using a FR4 Board to mount SMD Inductors and Capacitors. Board has an option to mount SMD device in the centre and SMA connectors are provided at the board edge. 50ohm trace connects SMD device and SMA connector. the test board is symmetric.

How to do In_Fixture TRL calibration for this Test board.

I have a through, open and short standard for the above fixture.
Can i cut a portion of the through board to make line standard.

Thanks,
Sridhar.  

Outcomes