AnsweredAssumed Answered

34411 auto zero and auto range time

Question asked by mikeatbosch on Jun 25, 2012
Latest reply on Jun 25, 2012 by mikeatbosch
I am setting a 34411 for 10 samples per (external) trigger.
I then need to set the sample timer.  The sample timer interval must include the actual integration/ measurement time--2 NPLC so 2 x 16.67ms.
But, how do I account for the auto zero and (if I use it) auto ranging times?

Thanks

Sorry I was interrupted, I believe that the meter will determine the Minimum sample time based on Auto range and zero on, the NPLC.  It can give you a recommended Min Sample Timer time.
Correct?

Edited by: mikeatbosch on Jun 25, 2012 12:28 PM  

Outcomes