AnsweredAssumed Answered

INPUT AND OUTPUT PORT LOSS DERIVATION

Question asked by ecrean on Jul 28, 2009
Latest reply on Jul 28, 2009 by daras
If I use an ECAL to calibrate the path to the DUT, is there an easy way to extract the path loss from the PNA to the DUT, and the path loss from the DUT to
the PNA?   With the E-CAL connected, can we extract the path loss to and from the DUT?  The reason I ask, is I would like to do a course power level cal without
a power meter.  Instead, I would asjust the PNA power based on the path loss to the DUT  

Outcomes