AnsweredAssumed Answered

cal fixture with response thru cal

Question asked by myonezaki on Sep 7, 2010
Latest reply on Sep 28, 2010 by Dr_joel
1-is it possible to use a s2p file with the cal-fixture simulator with the active measurement being a s21 measurement with only a response thru cal? 
2-as a quick check, if i selected a s2p file of a 3 dB attenuator as my fixture and the active measurement was a 2-port cal of a thru, with cal fixture sim on would i see a +3dB on s21?
3-is it possible to 'load' in a s21 file into 'memory' and perform a data/memory with the current measurement using a a cal-response thru?  previous attempt places the data from the s2p file into the memory in a different channel and not in the desired channel.
4-or what is the easist method to have a real time measurement -s21 with a cal-response thru having a fixture located on the output?
many thanks  

Outcomes