AnsweredAssumed Answered

How to do an LO source power cal programmatically?

Question asked by SteveE on May 5, 2006
Latest reply on May 5, 2006 by daras
I plan to use the E8362B PNA to make two stage Fixed Output Frequency SMC measurements with the LO1 source slaved to the PNA and the fixed LO2 source not controlled by the PNA. Using VEE I worked thru the VB example 'Create and Cal an SMC Measurement'. But it doesn't address how to make the LO source power calibration. Obviously it can be done manually thru the front panel LO source setup wizard, but I would like to be able to trigger and control it programmatical like the SMC cal.

Can it be done this way, and if so how?  

Outcomes