AnsweredAssumed Answered

2 separate C0 and L0 values in one calkit for PLTS v3.12?

Question asked by kentmallory on Nov 6, 2006
Latest reply on Nov 6, 2006 by odanzy
I have Cascade GSS probes, which specify different C0 and L0 terms for S1 (close to ground) and S2 (far from ground).  Anyone know of a work around allowing me to use both in PLTS?  Or would the best I could do is to put in only either S1 or S2 coefficients?

Currently my lab is not set up to use Wincal 2006 which I believe has all the functionality needed built in to correct for the offset ground.

Thanks,
Kent Mallory  

Outcomes