AnsweredAssumed Answered

The remote control problem in Agilent 8960

Question asked by jerrystone on Feb 8, 2012
Hi,

The problem is when I connect handheld device with 8960 successfully, the state of active cell shows "Attached", but I send GPIB command by LabVIEW to 8960, ex: CALL:BAND EGSM or CALL:BCH 38...etc, the state of active cell will change from "Attached" to "Idle". There is no this issue when I set BCH parameters by manual. Could anyone help me to solve it? thanks!

Jerry  

Outcomes