AnsweredAssumed Answered

What is Flush Thru Calibration?

Question asked by thangyw on Mar 16, 2006
Latest reply on Mar 17, 2006 by gfarrel
Can someone explain flush thru cal and when it is useful?

The PNA help file says:
FLUSH - When ECal calkits are specified, use the FLUSH THRU algorithm.  This selection has no affect if ECal calkits are not used or if the ECal module selected is not insertable.

Still dont understand what is explained in the help file

Thanks for the sharing,
"Learning is a weightless treasure you always carry easy"   HIPOWEREDPNA  

Outcomes