AnsweredAssumed Answered

PNA-L SCPI command to realize the Local lockout

Question asked by aldo09 on Nov 7, 2011
Latest reply on Nov 27, 2012 by odanzy
Hello,

I want to disable the use of the keyboard of my PNA.
I saw it was feasible by using the "LLO" command through a GPIB connection.
However I am connected with an Ethernet link.

It is noted in the doc that you can also do it by driving it via a LAN : "This feature is also supported using SICL over LAN".
But I can not find the equivalent command.

So I come to you because I need your help.
Thank you in advance.  

Outcomes