AnsweredAssumed Answered

calibration after reversing couplers

Question asked by matth on Jan 31, 2008
Latest reply on Feb 1, 2008 by dgun
In order to increase the dynamic range in my application, I have reversed both couplers on a E8362B ("rotation" of the jumpers of option 014). After a full two port SOLT calibration, I obtain error terms which look OK except both source match and load match at low frequency (-10dB at 10 MHz decreases below -20 dB only above 500 MHz). I find the same behavior on the uncorrected  return loss measured when a thru is connected between both ports (see attachment).

Is this behaviour normal ? (maybe are the receiver not so well impedance-matched at low frequency, which would explain why one measures so much reflected power when the receivers are directly connected to the main path of the couplers) or should I worry about that ?

Thank you in advance for your help  

Outcomes