AnsweredAssumed Answered

Need LabVIEW VIs for Agilent 4156C SMU

Question asked by shivam1985 on Aug 10, 2009
Latest reply on Oct 8, 2009 by Subhasis
I am using Agilent 4156C to measure the Id-Vd characteristics for MOSFET in sweep mode (i.e. for different constant gate voltage the variations of Id with Vd), so that I need three SMU connections as follows………

1.       SMU1: Vd (a start voltage, a stop voltage, sweep step)
2.       SMU2: Vg (a constant voltage)
3.       SMU3: common
Also we need an output graph for the corresponding measurement with the array for collecting data.

I am using LabVIEW for the same but the main problem is to setup the SMU connections. I have installed the drivers for 4156C and have made a program for SMU selection but that are not compatible with the drivers. Please help me out with this. Its urgent.  

Outcomes