We are using a customized testplan currently in 5.x. We have recently setup a dual-boot machine to work on upgrading to 7.10p. So far we have ran into a major stumbling block with 7.10p. Our testplans ask for operator input. However, we could use some advice on how to handle this in the GUI since there is only an output window for BT-basic.
1. Is it possible to create a msgbox asking for operator input?
2. I noticed that the migration presentation had a slide about running in a classic mode. I do not have audio capability, and was wondering how to set this up. Thanks
1. Is it possible to create a msgbox asking for operator input?
2. I noticed that the migration presentation had a slide about running in a classic mode. I do not have audio capability, and was wondering how to set this up. Thanks
I think 7.10p support the softkeys like what we used to have when running in the BT Basic window. Maybe that can help?
For classic mode, it is basically the BT-Basic mode. I think you can simply launch a BT-Basic window load in the testplan (get "testplan") and run it like what you do with 5.x software. Just don't launch the GUI.
But then, you lose the features that you get in the GUI like the Optimiser, Board browser, AutoDebug etc.