AnsweredAssumed Answered

Remotely listing installed options on E4406A

Question asked by bkoch709 on Sep 29, 2010
Latest reply on Oct 13, 2010 by tabbott
I want to be able to see the installed options on an E4406A VSA without having to physically look at the screen. Is there a GPIB command? Can this be done in NI MAX? I sedn the *OPT? command, but it sends the generic "BAC","B78" response. I want to see actual option numbers (ie. 204).  

Outcomes