I make a spectrum emission mask measurement (SEM) with PSA E4445A,and use the following command
":INST CDMA2K"
":CONF:SEM"
but while I send the command ":DISP:WIND:TRAC:Y:RLEV 10 DBM" ,change the reference level to 10 dBm,
PSA retuen a error message "-113,"Undefined header"
Does anybody know the solution?
thanks in advance.
":INST CDMA2K"
":CONF:SEM"
but while I send the command ":DISP:WIND:TRAC:Y:RLEV 10 DBM" ,change the reference level to 10 dBm,
PSA retuen a error message "-113,"Undefined header"
Does anybody know the solution?
thanks in advance.
but none of them works.My check steps are followed,
first,I operate the PSA using front panel key,
Mode-->CDMA2000,
Measure-->SEM,
Meas Setup--> Restore Meas Default,
Amplitude-->ref level 10 dbm
then I use SCPI command to read ref level
":DISP:SPEC:WIND:TRAC:Y:RLEV?" return 0
":DISP:SPEC1:WIND1:TRAC:Y:RLEV?" return 0
":DISP:SPEC1:WIND2:TRAC:Y:RLEV?" return 0
":DISP:SPEC3:WIND1:TRAC:Y:RLEV?" no response
":DISP:SPEC4:WIND1:TRAC:Y:RLEV?" no response
and I tried the following commands
":DISPlay:WAVeform[n]:WINDow[m]:TRACe:Y[:SCALe]:RLEVel<power>"
":DISPlay:WAVeform[n]:WINDow[m]:TRACe:Y[:SCALe]:RLEVel?"
None of them works too.
Does anybody know the solution and verify on the instrument?
Thanks
I'm pretty sure the ":DISP:WIND:TRAC:Y:RLEV 10 DBM" works in WCDMA SEM mode,too.
Could agilent add the command in CDMA2K SEM mode?