Hello,
Excuse me if I put my topic to bad place. We use SJ50 serie AOIs. I made a program which watches the .dat file and if an algorithm changes then my program makes a log file from the parameters of the modification. I know some numbers are which parameters, but I don't know all.
I write all:
DEVICE x
SEARCH 955 645
BOUND 0 0 0
BODY 590 300 0 0 0 0
LEADS 150 300 0 0 0 0
PADS 100 200 0 0 0 0
NUM_PINS 0 100 0 0
THRESH 80 98 110 65 50 0 0 0 0 0
FILTER 0 0 0 0
Colour 0 0 0 1 0 0 0 255
CAMDATA 51 2 0 0
EXTRA_p 0 1 0 0 100 100 0 0
PASTE 25 80 180 0 0 50 0 50
ALocation_p 0 50 160
Orient0 0 -600 400 100 0 0 0 0 0 0 0 0 0 ""
Somebody knows it which number exactly which parameter ? Thanks for your help!
Regards,
nkohler
Excuse me if I put my topic to bad place. We use SJ50 serie AOIs. I made a program which watches the .dat file and if an algorithm changes then my program makes a log file from the parameters of the modification. I know some numbers are which parameters, but I don't know all.
I write all:
DEVICE x
SEARCH 955 645
BOUND 0 0 0
BODY 590 300 0 0 0 0
LEADS 150 300 0 0 0 0
PADS 100 200 0 0 0 0
NUM_PINS 0 100 0 0
THRESH 80 98 110 65 50 0 0 0 0 0
FILTER 0 0 0 0
Colour 0 0 0 1 0 0 0 255
CAMDATA 51 2 0 0
EXTRA_p 0 1 0 0 100 100 0 0
PASTE 25 80 180 0 0 50 0 50
ALocation_p 0 50 160
Orient0 0 -600 400 100 0 0 0 0 0 0 0 0 0 ""
Somebody knows it which number exactly which parameter ? Thanks for your help!
Regards,
nkohler