AnsweredAssumed Answered

Operator screen activation

Question asked by dianar on Jul 14, 2010
Latest reply on May 18, 2011 by dbailey
On one machine we have three operator command windows and on the other, we only have two.  Is there a command to activate the third?

one machine has:
bt-basic window
graphical interface window
menu window along the top - listing "start" "stop" "quit" "fixture lock" etc.  (function keys)  this is the one that is missing on our other system  

Outcomes