AnsweredAssumed Answered

HP 8590B Option 1

Question asked by RFguy on Feb 6, 2012
Latest reply on Feb 6, 2012 by tabbott
I have a 8590B with option 001 and 003.  Just wondering if there is a way to internally convert from the 75 ohm option 1 to 50 ohm.  I know Pasternak makes an impedance matching connector (PE7028) that will convert 75 to 50, but I would like to avoid the additional connectors.

Also, I'm sure the impedance matching pads would probably introduce some loss in accuracy.

Any thoughts or help would be greatly appreciated!

Thanks  

Outcomes