AnsweredAssumed Answered

E4440A Total Harmonic Distortion software

Question asked by whitled on Sep 16, 2011
Latest reply on Oct 19, 2011 by tabbott
Wondering if someone may be able to shed some light on the question of...

Does the E4440A Harmonic Distortion "THD one-button automated measurement" display the result to the display screen or is the result only available in remote. I have firmware version A.11.16 Feb/11/2010 Opts 107,110,111,115,123,226,233,266, BAB

Using the analyzer from the front panel with a 50Mhz input CW, the CW harmonics are measured, but there is no display of the calculated total harmonic distortion. Is there supposed to be a displayed percentage or no? The results could be calculated by hand but is it supposed to be displayed?  

Outcomes