Hi,
I have two spectrum analyzer are HP8591A and HP8591E, Because need to send one spectrum analyzer (HP8591A or HP8591E) to another department. May you tell me What the different (Functions) between HP8591A and HP8591E?
I knew the price of HP8591E is higher then HP8591A, But my HP8591A its condition of the unit is very good.
Those HP8591A and HP8591E also have Option 004, 010 and 130
Thanks so much.
I have two spectrum analyzer are HP8591A and HP8591E, Because need to send one spectrum analyzer (HP8591A or HP8591E) to another department. May you tell me What the different (Functions) between HP8591A and HP8591E?
I knew the price of HP8591E is higher then HP8591A, But my HP8591A its condition of the unit is very good.
Those HP8591A and HP8591E also have Option 004, 010 and 130
Thanks so much.
It would probably be best if you did a side by side analyzer functionality comparison by viewing the User’s Guides on the Agilent.com website. Go to www.agilent.com and type in “8591A” in the search box, then select Technical Support, Manuals and you’ll see a listing there. You can do the same for the 8591E and then view the function similarities and differences. The manuals have a section dedicated to analyzer functions where a side by side can be done.
Basically, the 91E improved the 91A in many aspects from the mechanical design to added option functionality to instrument firmware enhancements to better specifications to an overhauled user interface.
If your measurements do not require the higher performance of the 91E, the 91A is a perfectly good spectrum analyzer that seems to withstand the test of time in many regards.
Regards -