All,
I am trying to set the X-Scale/Div remotely while the instrument is measuring Time Domain, where the measure time is 24mSec but I want to display 5mS worth of data on the waveform. So I need to set the X-scale to 500uS per/div. The only command I can find is X:PDIV dB. I also cannot find the command which should be referenced while the instrument is in the afformentioned mode. Any idea?
I am trying to set the X-Scale/Div remotely while the instrument is measuring Time Domain, where the measure time is 24mSec but I want to display 5mS worth of data on the waveform. So I need to set the X-scale to 500uS per/div. The only command I can find is X:PDIV dB. I also cannot find the command which should be referenced while the instrument is in the afformentioned mode. Any idea?
Not all of the remote display commands have been implemented in the PSA personalities. The work-around is to set up the measurement via the front panel and save a state. You can then recall the state remotely. Alternatively, you could just set up the measurement time to be 10 times the X-Scale/Div that you want, so that it auto scales to the X-Scale/Div that you want.
Hope this helped -