I need to adjust the above system. The service manual for the receiver 85462A and the test set 85460A shows automated adjustments. Does anybody know which sofware is used for that and is this software available?
While the service manuals for these receivers do refer to adjustment software, it was only made available to the HP/Agilent service centers. These instruments could be very complicated to service and adjust so the decision was made to limit the distribution of the adjustments...