Does a normal 70909A/910A operate with the 70590A Z40 ? What are the required modifications ? Apparently you have to reinstall the front input of the 909/910 to the rear but is a software modication necessary ? Thanks.
The 70590A option Z40 module was a special handling add-on that increased the upper frequency range of the 70909A from 26.5 GHz to 40 GHz. It would need to be enabled to work; however, it is out of support. The Agilent PSA spectrum analyzer can make measurements to 40GHz / 50 GHz. www.agilent.com/find/sa
The 70590A option Z40 module was a special handling add-on that increased the upper frequency range of the 70909A from 26.5 GHz to 40 GHz. It would need to be enabled to work; however, it is out of support. The Agilent PSA spectrum analyzer can make measurements to 40GHz / 50 GHz. www.agilent.com/find/sa
Regards -