I have HP8595E with option 41 (GPIB interface) but the SA does not recognize this option. I checked that physically I have correctly installed A40 board (08590-60366) but the SA does not lists this as one of the installed options. Is there a schematics available to debug this problem? Any troubleshooting guide? I can't find anything about this board in the Service Guide.
Any help appreciated.
Any help appreciated.
Also, just so you know, the option will not identify itself until the rear panel connector board is plugged in, as the board that goes inside the instrument is used for both options 041 and 043. Connecting the desired rear panel connector board will then make the correct identification of the option.
Best regards,
Mike