The option 009 allows connecting an external tracking generator on the spectrum.
I think that I can convert my HP8593E with option 009 myself because there is no board to add; just adding cable and connector to the back. I wish if someone could tell me where to find the description of that option with drawing...
Then I will looking to buy a tracking generator or a HP8350B sweeper (with module 592).
Thank you in advance
FM
I think that I can convert my HP8593E with option 009 myself because there is no board to add; just adding cable and connector to the back. I wish if someone could tell me where to find the description of that option with drawing...
Then I will looking to buy a tracking generator or a HP8350B sweeper (with module 592).
Thank you in advance
FM
5062-7710 W42 cable L.O. output
8120-5401 W48 cable Sweep + Tune output
link to the service for the 8590x series (674 pages I wouldn't try to print it). http://www.home.agilent.com/upload/cmc_ ... -90316.pdf
There's a block diagram that shows the connections, also parts listngs and all kinds of service info. Hope this gets you a little farther.
Steve