Hi
I am trying to carry out a modal test using an impact hammer on a space truss on a HP 35660A. The problem is that I just have the analyzer without any kind of documentation. Please if someone could help me out with the steps required to program the analyzer to get the Natural Frequency & phase.
I am trying to carry out a modal test using an impact hammer on a space truss on a HP 35660A. The problem is that I just have the analyzer without any kind of documentation. Please if someone could help me out with the steps required to program the analyzer to get the Natural Frequency & phase.
I'm not familiar with this analyzer, but I can tell you that the programming manual for it is on Agilent.com
35560A programming guide
http://cp.literature.agilent.com/litweb ... -90025.pdf
This manual has the commands you'll need, I'm not sure if you are also asking for help in setting up the measurement or in sending remote commands in general. Let us know.
Best regards,