Can anyone please offer advice as to where I might locate a DPDT 'RANGE' slide switch (HP P/N 3101-0070) for my HP8553b plug-in to the HP141T Spectrum Analyser. That switch is a bit flakey in my unit now. I know the unit is getting on in years but it is still quite OK for what I do. I am located in Australia but I am OK with buying stuff overseas.
If the original part is no longer available (which I suspect is the case) is there a well known equivalent.
Thanks
If the original part is no longer available (which I suspect is the case) is there a well known equivalent.
Thanks
I looked in our parts database and Agilent part number 3101-0070 is a double pole- double throw slide switch 0.5 A 125V with solder lugs. It is made by CW Industries as part number GF-126-0000.
I looked at DigiKey.com and there is a part with this part number sold there: http://parts.digikey.com/1/parts/974015 ... -0001.html
Regards -