I just bought an 8570A spectrum analyzer and obtained a pdf file of the 8559A manual from the internet. I am using the manual to adjust the 8559A manual unit since I think it is similar to the 8570A. The question I have is how to increase the gain of Band 3 (3.8-8.5 GHz) which is lower than the adjacent bands. I read the manual but am not sure what adjustment to make.