AnsweredAssumed Answered

Check if scope Triggered through GPIB

Question asked by DanHHunter on Jan 7, 2012
Latest reply on Jan 10, 2012 by flanguasco
Hello All!

First time poster... I was hoping I could get some help with an issue I'm having.

I'm having an issue with an old 54641A scope if it doesnt trigger because of an error from the UUT. If I'm testing the board and I dont meet the conditions to trigger the scope it gives me a GPIB error because I'm in single and normal mode checking for a single pulse, the scope doesnt have any information to give me when polled by the software thus causing the GPIB error. So I guess my question is how do I ask the scope if it has triggered?

Thanks for all your help in advance.

~Daniel  

Outcomes