AnsweredAssumed Answered

ECal orientation problem

Question asked by 68carlsson on Oct 11, 2006
Latest reply on Oct 13, 2006 by OsamuKusano
Have some Ecal problem when replacing the 8753 with ENA-L.
Have a amplifier setup with a 38dB attenuator between port 2 and the amplifier (DUT) output.
Doing a Enhanced Response ECal-calibration work just fine with the 8753 with auto orientation on.

Trying to do this with the ENA-L results in a "Module not in RF- path" message.
The only way to get this to work is to set orientation off and connect port 1 to Ecal port B and port 2 to Ecal port A.

It seems like the orientation algorithm is different between the 8753 and ENA-L.


One other comment is also that the described procedure for ENA-L is not possible to performed remotely.
I haven't been able to find the "orientation off" command. It's even hard to find the softkeys (Hidden in the service menu????).

In my opinion the ENA-L is still missing a lot of functionality available in the 8753. 

Does anyone have a solution?  

Outcomes