AnsweredAssumed Answered

1 PC & 2 PNA E835X

Question asked by kent on Jan 13, 2011
Latest reply on Jan 13, 2011 by andrew_cannon@keysight.com

Hi,

 

I'm looking for a procedure for configuring the proxy for two seperate PNA's on a local LAN.
The plan is to control both instruments via programming using C++.
The PNA Help C++ example shows how to establish a session for a single PNA that's been registered
using the proxy. However in my case when running the proxy setup for each PNA, the previous entries
are overwritten.

 

In code the example below would only work for one PNA. Is there a seperate method for opening a
session to the PNA by providing the hostname or ip address? I need some procedure or examples.

 

pNA = IApplicationPtr("AgilentPNA835x.Application.1");

 

Thanks in advance.  

Outcomes